Hello,
I'm planning a project with the MKL03Z. So I've ordered the FRDM-KL03Z board for testing. The problem is that I can't create a new Project in CodeWarrior 10.4 for the KL03Z-family. There are only the KL02Z, KL04Z and KL05Z available. Is the KL03Z supported?
regards
Sven
Hi Sven
The KL03 is a new part and these are supported by KDS [Kinetis Design Studio Integrated Development |Freescale] but not by CW10.x.
You can still build projects for the KL03 with CW but it is advisable to use KDS due to it containing the project/programming/debugging support.
Regards
Mark
KL03 - µTasker FRDM-KL03Z support
For the complete "out-of-the-box" Kinetis experience and faster time to market
Hello Mark,
I've downloaded the KDS 2.0 and have installed all updates. But the problem is the same as in CodeWarrior.
Regards
Sven
Adding new devices to KDS is a two step process: you need to download and install the Kinetis SDK first.
On
(use 'All downloads' on the right side)
Once you have it installed, use the KDS/Eclipse updater to add the device support with Help > Install New Software. Point it to
C:\Freescale\KSDK_1.0.0-KL03Z\tools\eclipse_update\
and update Eclipse from the zip file there.
Then you have KL03Z support listed:
I hope this helps,
Erich