imx6 sololite UART tx line activity while just receiving data

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 sololite UART tx line activity while just receiving data

659 Views
jagsgediya
Contributor II

Hi All,

We have a custom board based on the imx6 sololite.

We are facing the problem with the uart. We are just trying to receive the data through uart but when we are probing the Tx line, we are getting some garbage on it.

suppose I will do ,

cat /dev/ttymxc3

At this time also, I am getting some garbage on Tx line. Please help. What can be the reason?

Thanks,

Jags

Labels (4)
0 Kudos
2 Replies

486 Views
igorpadykov
NXP Employee
NXP Employee

Hi jags

reason may be short circuit with another signals,

recommended to test hardware UART lines

with i.MX 6Series Platform SDK

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

486 Views
maitegonzalez
Contributor I

Hello,

We are working with a custom board also and we are facing the same issue..

Any solution?? 

Thanks!

Maite

0 Kudos