HAB on imx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HAB on imx6

641 Views
saisuryanarayan
Contributor I

Hi freescale team,

Thanks for your fast reply.I followed your instructions and i am

not getting any HAB events.Now i fused HW_OCOTP_SRK(0-7) with fuse bianary

values.

Now my *hab_status *command not giving HAB events . In your

previous reply you told that make *SEC_CONFIG *to closed only after

checking all hab functions.

Now can you suggest me how to check HAB functions from

u-boot.In my u-boot i have only *hab_status *is available regarding HAB

check.

Checking hab_status is enough?

Do i need to check anything else before making SECURE_CONFIG to closed?

If yes please help me to check HAB functionality?

Thank You

With Warm Regards,

Sai Suryanarayan S

*Cell : *+91 8867185975 | Skype : Suryanarayan sarabu

0 Kudos
1 Reply

443 Views
Yuri
NXP Employee
NXP Employee

  Please use section 6.1 (Error Logging) of AN4581 (Secure Boot on i.MX50, i.MX53, and

i.MX 6 Series using HABv4 ). In particular, please pay attention on the example, which
"can be modified to also report all warning events, by using HAB_STS_ANY inhab_rvt_report_event,
instead of HAB_FAILURE".


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos