imx6 Quad core Evaluation Board to purchase

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 Quad core Evaluation Board to purchase

747 Views
lijothomas
Contributor II

Hi,

We are planning to use imx6Quad core processor for application;

Could any one suggest which is the right Evaluation board to procure to start with.

Is the MCIMX6Q-SDP is the right one to start ?

Our requirements are listed down,

Core : Quad

PCIe interface – Required 2 (can provide a PCI bridge if required)

Interfaces required:

CAN BUS    

  USB

UART           - 3 Nos.

SDIO            -> SDIO card Interface /  eMMC Interface

Gigabit Ethernet     -> 10/100/1000 GBE

GPIO           -> Pins with Interrupt Capability/ General IO

Display      -> TFT/ Touch Controller

Thanks & Regards

Lijo Thomas

Labels (1)
3 Replies

575 Views
igorpadykov
NXP Employee
NXP Employee

Hi Lijo

Sabre Auto best fit, since MCIMX6Q-SDP has not CAN

SABRE|Automotive-Infotainment|i.MX6|Freescale

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

575 Views
lijothomas
Contributor II

Thanks igor for the reply,

Do you have any other EB board to suggest, which has all the peripherals I mentioned

Regards

Lijo Thomas

0 Kudos

575 Views
igorpadykov
NXP Employee
NXP Employee

Hi Lijo

there are no other FSL reference boards with such

characteristics.

Best regards

igor