AnsweredAssumed Answered

CLOCK_SYS_GetBusClockFreq() returns 0 in KSDK 1.1

Question asked by Marco Hess on Feb 10, 2015
Latest reply on Feb 11, 2015 by Alice_Yang

I ported a project from KSDK 1.0 to 1.1 (in KDS 2.0) and am running into some trouble during the PDB initialisation.

 

Previously using KSDK 1.0, CLOCK_SYS_GetBusClockFreq() returned the correct 60MHz and I can calculate the correct PDB MOD value.

 

Now with KSDK 1.1 it returns 0.

 

I traced through the CLOCK_SYS_GetBusClockFreq() call but it goes through so many levels of lower level functions, I can't make sense of it anymore.

 

What's wrong?

Outcomes