Simultaneous firmware upgrade using MfgTools with imx233

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Simultaneous firmware upgrade using MfgTools with imx233

459 Views
paolomartinetti
Contributor I

Hi everybody,

i have a question about mfgtools:

is there any way to load one or more devices (imx233) simoultaneously with different profiles using mfgtools?

This question arises from the need to load different encrypted firmwares on different devices in a production environment.

Thanks in advance

Paolo

Labels (1)
0 Kudos
1 Reply

357 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Paolo,

Please check the Mfgtool operation manual documentation, in case of the latest mfgtool version 4.1v  refers that no more than 4 devices are allowed to be connected simultaneously. you need to check this manual according to the version  you are using, since previous mfgtools version are able to update firmware, in less than 4 devices

Have a great day,

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos