AnsweredAssumed Answered

Specifications of the I2S of RX of IMX6DL.

Question asked by Takashi Takahashi on Feb 9, 2015
Latest reply on Feb 9, 2015 by igorpadykov

Hi community.

 

Would you please tell me  about the specifications of the I2S of RX of IMX6DL.

Although we have with the current 16-bit received settings, what will happen to the behavior of if there is a data input of 24-bit?

 

[The reason]

Our customer use 24-bit output only supports devices with  external devices.

Manufacturers responded ,only 16-bit loads is no problem and without the lower 8-bit.

 

[Question and specification expect]

As a specification of IMX6DL, 

The capture only 16-bit data of register set in the 24-bit data, What possible lower 8-bit is set to ignore (Do not care)?

 

 

Outcomes