WM8962 POWER FAILE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

WM8962 POWER FAILE

527 Views
kimsangyoung
Contributor I

Deare anyone

There are testing a new board i.mx 6q cpu comes with the following message on the console .

Power DCVDD g2 of wm8962 pin is properly entered. Why can output this message?

Audio clock MCLK 24MHZ to use I.MX6Q do I get from the setting to use an external clock register ?

CONSOL MEASSAGE

+++++++++++++++++++++++++++++++++++++++++++++

wm8962 0-001a: Failed to get supply 'DCVDD': -19

wm8962 0-001a: Failed to request supplies: -19

 

Labels (1)
0 Kudos
1 Reply

342 Views
igorpadykov
NXP Employee
NXP Employee

Hi kim

seems this error was solved on below link

Question about WM8962 without PMPF0100 PMIC.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos