Need the source code of 'tvsrc' (libmfw_gst_tvsrc.so)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need the source code of 'tvsrc' (libmfw_gst_tvsrc.so)

Jump to solution
847 Views
RobbieJiang
Contributor IV

Hi,

Currently the 'tvsrc' element works with my CSI camera on MX6Q/Linux platform.

However, we would like to make some changes to 'tvsrc', e.g, to add some new attributes,

or to support more input resolutions.

So the source code of 'tvsrc' is needed.

But I have only the binary code of libmfw_gst_tvsrc.so,

where can I get the source code?

Regards,

Jie

Labels (3)
1 Solution
594 Views
igorpadykov
NXP Employee
NXP Employee

Hi Robbie

in gst-fsl-plugins-3.0.11.tar.gz I found

1.jpg

2.jpg

~igor

View solution in original post

4 Replies
594 Views
igorpadykov
NXP Employee
NXP Employee

Hi Robbie

had you looked in gst-fsl-plugins L3.0.35_4.1.0_MM_CODECS

Middleware-Codecs and other Algorithms (11)

i.MX6Q|i.MX 6Quad Processors|Quad Core|Freescale

Best regards

igor

0 Kudos
594 Views
RobbieJiang
Contributor IV

Hi igor,

In the codecs packaged you mentioned,

there is no source code for tvsrc.

Is it a third party software?

Why is fsl's 'mfw_v4lsrc'  not used and replaced by tvsrc?

Regards,

Robbie

0 Kudos
595 Views
igorpadykov
NXP Employee
NXP Employee

Hi Robbie

in gst-fsl-plugins-3.0.11.tar.gz I found

1.jpg

2.jpg

~igor

594 Views
RobbieJiang
Contributor IV

Hi igor,

Thanks for your information.

I tried to download  L3.0.35_4.1.0_MM_CODECS,

but actually it is included in L3.0.101_4.1.1_MM_CODECS.

Anyway,  thanks a lot!

Regards,

Jie

0 Kudos