AnsweredAssumed Answered

Question, i.MX6S camera inputs

Question asked by AVNET JAPAN FAE (team share account) on Feb 8, 2015
Latest reply on Feb 9, 2015 by igorpadykov

Dear team,

 

I would like to ask about camera input of i.MX6Solo.

Can i.MX6 Solo support two camera channels that are connected to parallel port CSI o i.MX6 Solo at the same time?

Referring to the schematics of i.MX6 SABRE AI Base board, we can find the AD7180 is used for two camera inputs and sending out to CSI0 parallel of i.MX6.

In the case of using one CSI parallel port of i.MX6S, can multiple camera streams be handled by i.MX6S?

If possible, how many camera inputs at the maximum can be handled in such case?

My customer wants to feed multiple camera data into i.MX6S and record the multiple streams to storage device.

 

Thanks,

Miyamoto

Outcomes