About booting from eMMC5.0 Device for i.MX6.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About booting from eMMC5.0 Device for i.MX6.

Jump to solution
1,183 Views
yuuki
Senior Contributor II

Dear all,

An eMMC5.0 device is used in our system.


We referred to the following URL, and changed a value of "card->ext_csd.rev ".
https://community.freescale.com/message/435796#435796

After booting from SD, OS is able to access the eMMC5.0 device.
However, when our system boots from eMMC5.0 device, that's failed.

If it was eMMC4.5 device, it succeeded.

Does BootROM of MX6 support eMMC5.0?
Does BootROM check EXT_CSD_REV of eMMC?

Best Regards,
Yuuki

Labels (1)
1 Solution
453 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

BootROM of MX6QD checks EXT_CSD_REV, but it does not support eMMC5.0

and fall back to flow for eMMC4.4. In general, one can try solutions on link below

eMMC 8GB to 4GB - crash on linux (yocto) boot

Best regards

igor
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
454 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

BootROM of MX6QD checks EXT_CSD_REV, but it does not support eMMC5.0

and fall back to flow for eMMC4.4. In general, one can try solutions on link below

eMMC 8GB to 4GB - crash on linux (yocto) boot

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos