Hi community,
Our partner have a question about i.MX6S eCSPI BIT_COUND and BUSRT_LENGTH.
Please see the questions as below.
[Q1]
"BIT_COUNT" is mentioned in "21.7.3 Transmit Data Register (ECSPIx_TXDATA)" of reference manual (IMX6SDLRM Rev.1).
But, we can not find the bit field in "21.7.4 Control Register (ECSPIx_CONREG)" of reference manual.
I think "BIT_COUNT" is a misprint, "BURST_LENGTH" is correct, right?
[Q2]
Description of "BURST_LENGTH" is up to "2^7 words" written in "21.7.4 Control Register (ECSPIx_CONREG) Bit31:20" of reference manual.
We think this description shows "128 words", but we think there are only 64 words in FIFO.
Can you tell us relation of "BURST_LENGTH" and FIFO ?
Best Regards,
Satoshi Shimoda
Solved! Go to Solution.
Please look at my comments below.
1.
Yes, it is assumed, that the BIT_COUNT is BURST_LENGTH.
2.
FIFO size is less than the BURST_LENGTH : a transaction is not considered as
finished (SS is asserted) while all bits, defined via the field BURST_LENGTH, are
not transferred – with waiting (if needed) TXFIFO filling dynamically (during transfer).
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Please look at my comments below.
1.
Yes, it is assumed, that the BIT_COUNT is BURST_LENGTH.
2.
FIFO size is less than the BURST_LENGTH : a transaction is not considered as
finished (SS is asserted) while all bits, defined via the field BURST_LENGTH, are
not transferred – with waiting (if needed) TXFIFO filling dynamically (during transfer).
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------