AnsweredAssumed Answered

Issue with SSL_Connect on QEMU

Question asked by Navin Daga on Feb 5, 2015

I'm using QorIQ Linux SDK v1.6 which has openssl version 1.0.1g. The host OS is CentOS 7.

 

I run QEMU emulation using qemu-system-ppc64 and I have not been able to establish SSL connection to a server. SSL Connection works from the host system but does not work on QEMU.

 

Any suggestions?

 

I use openssl s_client to test connection to the server and on QEMU, it reports :

"error:140790E5:SSL routines:SSL23_WRITE:ssl handshake failure:s23_lib.c:177:"

Outcomes