AnsweredAssumed Answered

How do I connect Connect windows 8.1  adb to imx6 android demo 4.2.2 on SABRE Board Reference Design|Freescale

Question asked by dcio deviceCloud.io on Feb 3, 2015
Latest reply on Feb 16, 2015 by CarlosCasillas

Hi,

 

I can't get ADB to list the device.

Here are the details

1. Host PC -- windows 8.1 , Android SDK installed. (SDK tools Rev 24.0.2, SDK platform tools Rev 21, google USB driver Rev 11.0)

2  Device  -- SABRE Board Reference Design|Freescale

   Device is running Android 4.2.2 demo image received on the SD card shipped with the board.

   kernel version 3.0.35-06114-g3b96084,  enrique@enrique-desktop#1 , Sat May 11 10:48:26 CDT 2013, Build number 1.0.0-rc3.

3.  The Developer options Stay Awake and USB debugging are enabled on the tablet.

4. I have followed all the steps in QSG guide as well as steps listed in similar threads in the community

 

Device Manager on HOST PC indicates device is functioning normally and device shows up as Andorid Device->Android ADB Interface with following details.

 

Device USB\VID_18D1&PID_0D02\0123456789ABCDEF was configured.

 

Driver Name: usb.inf

 

Class Guid: {36FC9E60-C465-11CF-8056-444553540000}

 

Driver Date: 06/21/2006

 

Driver Version: 6.3.9600.17238

 

Driver Provider: Microsoft

 

Driver Section: Composite.Dev.NT

 

Driver Rank: 0xFF2003

 

Matching Device Id: USB\COMPOSITE

 

Outranked Drivers:

 

Device Updated: false

 

---------------------

5. I tried to use the android_usb_fsl.zip from R10.3 as well as R10.4

   but driver installation fails with errror

"The folder you specified doesn't contain compatible software driver for your device.

If the folder contains a driver, make sure it is designed to with Windows for x64-based systems".

6. android adb_usb.ini has been updated for VID 0x18D1 as well as 0x15A2

7. google USB driver install/unintall tried multiple times.

8. Connect adb to imx6 android demo 4.4.2  thread has exactly same problem, but no working solution

8. Connected debug port and observe following logs during system boot

 

init: cannot find '/system/etc/install-recovery.sh', disabling 'flash_recovery'

 

android_work: sent uevent USB_STATE=CONNECTED

 

android_work: sent uevent USB_STATE=DISCONNECTED

 

android_usb: already disabled

 

android_usb: already disabled

 

mtp_bind_config

 

adb_bind_config

 

warning: `adbd' uses 32-bit capabilities (legacy support in use)

 

adb_open

 

android_work: sent uevent USB_STATE=CONNECTED

 

input: eCompass as /devices/virtual/input/input9

 

android_usb gadget: high speed config #1: android

 

android_work: sent uevent USB_STATE=CONFIGURED

 

root@android:/ # imx-ipuv3 imx-ipuv3.0: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)

 

request_suspend_state: wakeup (3->0) at 19189905005 (2015-02-03 07:15:45.283076336 UTC)

 

cpufreq_interactive_input_connect: connect to max11801_ts

 

cpufreq_interactive_input_connect: connect to eGalax Touch Screen

 

mma enable setting active

 

eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=1:01, irq=-1)

 

ADDRCONF(NETDEV_UP): eth0: link is not ready

 

Compat-wireless backport release: patch-10-27-gd46416c-p

 

Backport based on  branching-msm-3.2.3-44-g65b285b

 

Calling CRDA to update world regulatory domain

 

World regulatory domain updated:

 

    (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp)

 

    (2402000 KHz - 2472000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)

 

    (2457000 KHz - 2482000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)

 

    (2474000 KHz - 2494000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)

 

    (5140000 KHz - 5360000 KHz @ 40000 KHz), (N/A, 3000 mBm)

 

    (5460000 KHz - 5860000 KHz @ 40000 KHz), (N/A, 3000 mBm)

 

android_readwrite_file: ret=-2

 

android_readwrite_file: ret=-2

 

acc_open

 

acc_release

 

ehci_fsl_bus_resume begins, Host 1

 

ehci_fsl_bus_resume ends, Host 1

 

ehci_fsl_bus_resume begins, DR

 

mtp_open

 

PHY: 1:01 - Link is Up - 100/Full

 

ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready

 

ehci_fsl_bus_suspend begins, Host 1

 

ehci_fsl_bus_suspend ends, Host 1

 

timeout while waiting for init operation

 

init: sys_prop: permission denied uid:1003  name:service.bootanim.exit

 

 

 

root@android:/ #

 

root@android:/ # android_readwrite_file: ret=-2

 

android_readwrite_file: ret=-2

 

mtp_release

 

mtp_open

 

adb_release

 

mtp_release

 

android_usb: already disabled

 

android_usb: already disabled

 

mtp_bind_config

 

adb_bind_config

 

adb_open

 

android_work: sent uevent USB_STATE=DISCONNECTED

 

android_work: sent uevent USB_STATE=CONNECTED

 

android_usb gadget: high speed config #1: android

 

android_work: sent uevent USB_STATE=CONFIGURED

 

mtp_open

 

adb_release

 

mtp_release

 

android_usb: already disabled

 

android_usb: already disabled

 

mtp_bind_config

 

adb_bind_config

 

init: untracked pid 3681 exited

 

adb_open

 

android_work: sent uevent USB_STATE=DISCONNECTED

 

android_work: sent uevent USB_STATE=CONNECTED

 

android_usb gadget: high speed config #1: android

 

android_work: sent uevent USB_STATE=CONFIGURED

 

mtp_open

 

 

---------------------

 

Could you please help

Outcomes