Hi,
I have a simple question about the correct kernel config option for iMX53 NAND NFC support. Should CONFIG_MTD_NAND_IMX_NFC should be enabled in the kernel?
The reason I ask is that the imx5_defconfig file (which supports MX53 NAND) does not have it set yet it looks like it should be set. Here's the relevant piece of the config file
Can someone clarify this?
Thanks,
Bruno
Solved! Go to Solution.
Hi Bruno
CONFIG_MTD_NAND_IMX_NFC was
for older NFC revisions used in i.MX21,MX31.
Best regards
igor
Hi Bruno
I believe not since one has already CONFIG_MTD_NAND_MXC_V3=y,
also refer to attached file. In ltib build one can select ard board,
it has nand support
L2.6.35_11.05_ER_SOURCE : Linux 2.6.35 Source Code Files and documentation 11.05 for i.MX53 SABRE Tablet.
Best regards
igor
Hi Igor,
OK. It looks like CONFIG_MTD_NAND_MXC_V3=y is the correct configuration option to use the iMX53 NAND Flash Controller.
I'm just curious what CONFIG_MTD_NAND_IMX_NFC is used for?
Bruno
Hi Bruno
CONFIG_MTD_NAND_IMX_NFC was
for older NFC revisions used in i.MX21,MX31.
Best regards
igor