Hi everyone.
I want to install the linux on i.MX6 Board.
What need for install? and How to install linux for i.MX6?
please help
Thank you to read.
Solved! Go to Solution.
H JooWon
you can two alternatives, first yocto (also please read attached Freescale_Yocto_Project_User's_Guide.pdf)
L3.10.53_1.1.0_iMX6QDLS_Bundle : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite,
i.MX 6Solo Linux Binary Demo Files and Linux BSP Documentation
second - ltib, for that first read below appnote
http://cache.freescale.com/files/dsp/doc/app_note/AN3875.pdf
the attached files
L3.0.35_4.1.0_ER_SOURCE_BSP : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite,
i.MX 6Solo and i.MX 6Sololite Linux BSP Source Code Files.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
H JooWon
you can two alternatives, first yocto (also please read attached Freescale_Yocto_Project_User's_Guide.pdf)
L3.10.53_1.1.0_iMX6QDLS_Bundle : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite,
i.MX 6Solo Linux Binary Demo Files and Linux BSP Documentation
second - ltib, for that first read below appnote
http://cache.freescale.com/files/dsp/doc/app_note/AN3875.pdf
the attached files
L3.0.35_4.1.0_ER_SOURCE_BSP : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite,
i.MX 6Solo and i.MX 6Sololite Linux BSP Source Code Files.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igorpadykov
Thank you reply.
If install the linux on i.MX Board, could operating without SDcard?
thank you.
JooWon
Hi JooWon
SD is needed for rootfs, also one can use NAND or nfs instead SD.
Please read Linux User Guide for available options.
~igor