AnsweredAssumed Answered

Mounting SD card with FAT32 file system in T1040RDB board through onboard SD card slot.

Question asked by Abhinav Bipnesh on Jan 29, 2015
Latest reply on Feb 3, 2015 by Yiping Wang

Hi,

 

Currently I am running fsl-image-core on T1040RDB board using NFS boot. I was trying to mount the SD card (which I have put in on board SD slot). The file system is FAT32 on that card. So I am not able to find how to mount that SD card in the OS. Do I need to re-compile the kernel to support for FAT32 and also SD card.

Please suggest on the same.

 

-Abhinav

Outcomes