Hello,
My customer has purchased this Freescale i.MX53 Sabre Tablet.
Previously, they are unable to find any update on the development platform which include various source codes and device drivers which is required to build the system before they are able to talk to various flavors of Android which lie on the top of embedded LINUX operating system.
Just wondering if FSL managed to release any new software platform?
Seems like there is not much update since 2013.
Thanks for your time for replying my questions.
Hi Allen
latest official BSP releases can be found on link below
SABRE Platform for Tablets Reference Design|Freescale
Also one can use community software, links below, these are
more frequently updated.
FSL Community BSP Release Notes 1.7 documentation
http://freescale.github.io/doc/release-notes/1.7/index.html
Index of /releases/yocto/yocto-1.6/machines/imx53qsb
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------