i.MX6Q Dual display

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Q Dual display

Jump to solution
1,113 Views
JHY
Contributor IV

I have confused i.mx6q dual display options.

Please tell me the answer for below yes/no questions.

It will be run in linux or android.

1. Same image Same resolution (ex. 1280x720 in LVDS and 1280x720 HDMI) <- maybe yes

2. Same image Different resolution (ex. 1280x720 in LVDS and 1920x1080 HDMI)

3. Different image Same resolution (ex. 1280x720 in LVDS and 1280x720 HDMI and different image)

4. Different image Dirrerent resolution (ex. 1280x720 in LVDS and 1920x1080 HDMI and different image)

Thank you.

Labels (1)
1 Solution
630 Views
igorpadykov
NXP Employee
NXP Employee

Hi JHY

this depends on what do you mean.

How many fps and how they are connected to

IPUs (one IPU for two LCDs or two IPU, one per LCD)

Best regards

igor

View solution in original post

0 Kudos
3 Replies
630 Views
igorpadykov
NXP Employee
NXP Employee

Hi JHY

below theoretical capability per one IPU

MX6 IPU.jpg

however real application may have less capabilities due to

processor/memory bandwidth limitations.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

630 Views
JHY
Contributor IV

Thank you for your reply.

But I am not sure that HD720 + HD1080 dual display is possible.

How can I determine for that?

0 Kudos
631 Views
igorpadykov
NXP Employee
NXP Employee

Hi JHY

this depends on what do you mean.

How many fps and how they are connected to

IPUs (one IPU for two LCDs or two IPU, one per LCD)

Best regards

igor

0 Kudos