AnsweredAssumed Answered

AIC LOOPBACK DEMO EXAMPLE DOES NOT WORK

Question asked by RC Reddy on Jan 21, 2015
Latest reply on Feb 20, 2015 by David Li

Hi,

   I ran the test [as a binary image from linux] and all i get is this

 

/ipc/dsp_bt aic_loopback_9x31_dbg.bin

===DSP boot Application===(1.1.01)==

SYSTEM MAP

DSP PrivArea: Addr=38000000 Size=8000000

Shared CtrlArea: Addr=37000000 Size=1000000

DSP Core0 M2: Addr=b0000000 Size=80000

DSP Core1 M2: Addr=0 Size=0

DSP M3: Addr=0 Size=0

PA CCSRBAR: Addr =ff700000 Size=100000

DSP CCSRBAR: Addr =ff600000 Size=100000

PA Shared Area: Addr=20000000 Size=f000000

DSP Shared Area: Addr=2f000000 Size=1000000

DSP READY SET

 

 

Copy Part b0000000 206d6

 

 

Copy Part b0024000 2f74

 

 

Copy Part ff618108 4

 

 

DSP HW Sem1 value not correctly set, value=0

 

 

DSP Boot Failed, Please reset

 

=============

I DONT see any prints as put in the console of the RDB board. I went through the code, and the code has good amount of printf statements.

 

 

as part of README.txt, it says following

 

a. Run Linux boot

b. Run Linux PA side AIC scripts

 

i don't see any PA side AIC scripts, where can i find those, please help.

 

Thanks

RC Reddy

Outcomes