Difference between the "Cross ARM C++ Compiler" and the "GNU ARM C++ Compiler"?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Difference between the "Cross ARM C++ Compiler" and the "GNU ARM C++ Compiler"?

1,066 Views
tharonhall
Contributor IV

It was suggested to me that the "Cross ARM C++ Compiler" is unique to KDS, and I should ask my question here:

 

Original Question:

 

What is the difference between the "Cross ARM C++ Compiler" and the "GNU ARM C++ Compiler"?

 

Is it a fork of the GNU? Does it support the same commands and pragmas as GNU?

 

I've had ZERO luck Googling this.

 

--------------------

Follow up Post:

 

I can note that since I posted this, I did see a comment somewhere that the Cross Compiler is derived from the GNU Compiler, but no explanation was given as to what the differences are.

 

Labels (1)
0 Kudos
0 Replies