Response on IMX6 solo board is deadly slow

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Response on IMX6 solo board is deadly slow

583 Views
swaraj
Contributor II

Hi,

I got wandboard with IMX6 solo processor on it, it had Ubuntu 11.04 version OS image built on it.

MY IMX6 board is responding very slowly and cannot open GUI at all.

Sometimes I see mmcqd/0 process is consuming too much of CPU.

Can anybody suggest me in resolving this issue.

Thanks,

Swaraj

Labels (3)
0 Kudos
1 Reply

423 Views
SergioSolis
NXP Employee
NXP Employee

I'm not familiar with the wandboard but probably the BSP is not enabled for graphics acceleration, since the CPU is working at full it could be that it is doing all the graphics processing by software rather than hardware.

Have you checked on the wandboard forums to check if their BSP has an update?

0 Kudos