AnsweredAssumed Answered

how to install zlib for ltib installation ..??

Question asked by Viswanath kondapalli on Jan 19, 2015
Latest reply on Jul 22, 2016 by Dumitru Popa

HP-xw4400-Workstation:~/Desktop/L3.0.35_4.1.0_130816_source/ltid/ltib$ ./ltib

defined(@array) is deprecated at /home/cyient/Desktop/L3.0.35_4.1.0_130816_source/ltid/ltib/bin/Ltibutils.pm line 362.

    (Maybe you should just omit the defined()?)

 

ltib cannot be run because one or more of the host packages needed to run it

are either missing or out of date or not in ltib's standard path.  Please

install/upgrade these packages on your host.  If you have your own utilities

in non-standard paths, please add an entry into the .ltibrc file for example:

 

%path_std

/usr/local/bin:/usr/bin:/bin:/usr/bin/X11:/usr/X11R6/bin:/my/own/exes

 

Package                Minimum ver   Installed info

-------                -----------   ---------------

zlib                   0             not installed

 

Died at ./ltib line 1409.

traceback:

main::host_checks:1409

  main:554

 

 

Started: Tue Jan 20 11:45:13 2015

Ended:   Tue Jan 20 11:45:15 2015

Elapsed: 2 seconds

 

 

Build Failed

 

Exiting on error or interrupt

Outcomes