YUV422 out put with HDMI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

YUV422 out put with HDMI

Jump to solution
2,946 Views
takashitakahash
Contributor III

Hi community.

Our partner has question.

Would you please teach me  how to set the data.

For H.264 (YCrCb420) video data is output from the HDMI as a YUV422.

what can be realized as performing any processing.

Labels (3)
0 Kudos
1 Solution
1,986 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
5 Replies
1,987 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
1,989 Views
YixingKong
Senior Contributor IV

Takashi-san

We are sorry for the delay. This support request has been assigned to AE team. If you do not se response in 3 days, please contact me again.

Thanks,

Yixnig

0 Kudos
1,989 Views
saurabh206
Senior Contributor III

Hi,

You can do YUV420 to YUV422 conversion using IPU.

Thanks

Saurabh

0 Kudos
1,989 Views
takashitakahash
Contributor III

Hi

Thank you for your replay.

I understand the IPU can be converted  YcrCb 4:02 to YUV422 possible.

Pleased to advice on how to convert and what register setting with HDMI.

0 Kudos
1,989 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

Hi Takashi, you can run the followed command to switch HDMI output between YUV and RGB format:

// Switch to YUV output mode

$ echo 0 > /sys/devices/platform/mxc_hdmi/rgb_out_enable

// Switch to RGB output mode

$ echo 1 > /sys/devices/platform/mxc_hdmi/rgb_out_enable