efk wrote:
What is the standard firmware uploading procedure for production ?
I've been thinking about the same myself.I've modified my generic JTAG programmer to do EzPort and I was wondering if there is a demand for such a programmer. What do other 52235x users think?
I can think of three possible methods
1) BDM
2) EzPort
3) EzPort through JTAG where the EzPort is connected to some other JTAG device1 and 2 has the disadvantage that it requires a connector (BDM being quite bulky) in addition to JTAG (or some clever muxing). The operator has to plug/unplug these under production. One can of course make some kind of edge-connector etc. on the board to eliminate the cost of the connectors. 3 is a problem if there are no other JTAG parts on the board, even though adding one is a possibility (the cheapest I can think of is the Xilinx Coolrunner II which cost 1$ in low quantities).