i.MX6DualLite : USB_H1_VBUS behavior on unpowered processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6DualLite : USB_H1_VBUS behavior on unpowered processor

Jump to solution
966 Views
koichisakagami
Contributor II

Dear community,

We are investigating the USB_H1_VBUS  behavior on custom board.

We know that
In i.MX6 USB VBUS can be powered any time,even to unpowered processor
from IMX6DLIEC sect.4.2.1 Power-Up Sequence.
USB_OTG_VBUS and USB_H1_VBUS are not part of the power supply
sequence and can be powered at any time.

[Background]
In the case of the i.MX6 powers off ,while the USB_OTG_VBUS is added with 5V,
the USB_H1_VBUS remains about 5 V.

When the i.MX6 powers off, on impressing a 5V to  the USB_OTG_VBUS,
the USB_H1_VBUS remains about 5 V.

Meantime,
in the case of  i.MX6 never power on ,
even if the USB_OTG_VBUS is added with 5V,
the USB_H1_VBUS does not appear 5 V.

[Question]
We think that this behavior is caused for the description in the datasheet IMX6SDLIEC 4.3.2.3 LDO_USB.
Is my understanding right ?

Best Regards,
Koichi Sakagami

Labels (1)
0 Kudos
1 Solution
489 Views
art
NXP Employee
NXP Employee

Yes, your understanding is correct.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
490 Views
art
NXP Employee
NXP Employee

Yes, your understanding is correct.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
489 Views
宗標廖
Contributor V

 

 

0 Kudos