AnsweredAssumed Answered

httpsrv gzip compression

Question asked by seandema on Jan 16, 2015
Latest reply on Dec 15, 2015 by Adrian Rockall

I'm running MQX 4.1.0.1 on a Kinetis K60 and attempting to use compressed files stored in TFS running on the built in RTCS web server. However I'm having some trouble getting it to work with compressed files. My page loads fine if I decompress the files leading me to believe the webpage code is ok. But if I have files compressed (in .gz or .zip) the web page does not display correctly.

 

I have 4 files, 1 .html, 2 .js and 1 .css file. I have gzip compressed the .css and .js files. So they now have a .js.gz or .css.gz style file name. I realize .gz is not supported by default but using the supported .zip does not work either. The page loads just as poorly with both.

 

Following the instructions listed here Re: Re: How to set Content Disposition? I have added support for .gz files. I'm guess I did this ok since it at least works the same as the included .zip support.

 

typedef enum httpsrv_content_type
{
    HTTPSRV_CONTENT_TYPE_OCTETSTREAM = 1,
    HTTPSRV_CONTENT_TYPE_PLAIN,
    HTTPSRV_CONTENT_TYPE_HTML,
    HTTPSRV_CONTENT_TYPE_CSS,
    HTTPSRV_CONTENT_TYPE_GIF,
    HTTPSRV_CONTENT_TYPE_JPG,
    HTTPSRV_CONTENT_TYPE_PNG,
    HTTPSRV_CONTENT_TYPE_JS,
    HTTPSRV_CONTENT_TYPE_ZIP,
    HTTPSRV_CONTENT_TYPE_PDF,
    HTTPSRV_CONTENT_TYPE_GZIP,
} HTTPSRV_CONTENT_TYPE;

 

static const httpsrv_table_row content_type[] = {
        { HTTPSRV_CONTENT_TYPE_PLAIN,       "text/plain" },
        { HTTPSRV_CONTENT_TYPE_HTML,        "text/html" },
        { HTTPSRV_CONTENT_TYPE_CSS,         "text/css" },
        { HTTPSRV_CONTENT_TYPE_GIF,         "image/gif" },
        { HTTPSRV_CONTENT_TYPE_JPG,         "image/jpeg" },
        { HTTPSRV_CONTENT_TYPE_PNG,         "image/png" },
        { HTTPSRV_CONTENT_TYPE_JS,          "application/javascript" },
        { HTTPSRV_CONTENT_TYPE_ZIP,         "application/zip" },
        { HTTPSRV_CONTENT_TYPE_GZIP,        "application/x-gzip" },
        { HTTPSRV_CONTENT_TYPE_PDF,         "application/pdf" },
        { HTTPSRV_CONTENT_TYPE_OCTETSTREAM, "application/octet-stream" },
        { 0,    0 }
};

 

static httpsrv_content_table_row content_tbl[] = {
    /* Size,          extension, MIME type,                        Cache? */
    {sizeof("js")-1 ,   "js",    HTTPSRV_CONTENT_TYPE_JS,          TRUE},
    {sizeof("gz")-1,    "gz",    HTTPSRV_CONTENT_TYPE_GZIP,        FALSE},
    {sizeof("css")-1,   "css",   HTTPSRV_CONTENT_TYPE_CSS,         TRUE},
    {sizeof("gif")-1,   "gif",   HTTPSRV_CONTENT_TYPE_GIF,         TRUE}, 
    {sizeof("htm")-1,   "htm",   HTTPSRV_CONTENT_TYPE_HTML,        TRUE},
    {sizeof("jpg")-1,   "jpg",   HTTPSRV_CONTENT_TYPE_JPG,         TRUE},
    {sizeof("pdf")-1,   "pdf",   HTTPSRV_CONTENT_TYPE_PDF,         FALSE}, 
    {sizeof("png")-1,   "png",   HTTPSRV_CONTENT_TYPE_PNG,         TRUE},
    {sizeof("txt")-1,   "txt",   HTTPSRV_CONTENT_TYPE_PLAIN,       FALSE},
    {sizeof("zip")-1,   "zip",   HTTPSRV_CONTENT_TYPE_ZIP,         FALSE},
    {sizeof("html")-1,  "html",  HTTPSRV_CONTENT_TYPE_HTML,        TRUE},
    {sizeof("shtm")-1,  "shtm",  HTTPSRV_CONTENT_TYPE_HTML,        FALSE},
    {sizeof("shtml")-1, "shtml", HTTPSRV_CONTENT_TYPE_HTML,        FALSE},
    /* Following row MUST have length set to zero so we have proper array termination */
    {0,                      "", HTTPSRV_CONTENT_TYPE_OCTETSTREAM, FALSE}
};

 

I'm not an expert on the inner working of RTCS or the web server but is there anything else I need to do to enable support for compression?

 

Thanks,

Sean

Outcomes