AnsweredAssumed Answered

bug in debug console for FRDM-K22F BOARD_DEBUG_UART_INSTANCE?

Question asked by christophertschappatt on Jan 15, 2015
Latest reply on Feb 13, 2015 by David E Seymour

This is in KSDK 1.1.0 and I am wondering if this is a bug. I had to change the statement "#define BOARD_DEBUG_UART_INSTANCE 2"  to "#define BOARD_DEBUG_UART_INSTANCE 1" in DbgCs1.h for my debug_printf command to write to 0x4006b000 instead of 0x4006c000 which was not working. I set the device to UART1 so that it would write to PTE0 so that I can use the pins that go to the UART that goes to the USB debug port but that was not sufficient.


Outcomes