AnsweredAssumed Answered

yocto bitbake build freezes at recipe qt4-x11-free-1_4.8.5-r0: task do_compile: Started

Question asked by Alvin Dizon on Jan 13, 2015
Latest reply on Jan 18, 2015 by Alvin Dizon

Hello,

I am building an image using the "bitbake fsl-image-x11" command. Bitbake seems to run through all the tasks but the output freezes at "recipe qt4-x11-free-1_4.8.5-r0: task do_compile: Started". I have tried stopping bitbake and rebuilding, but it always stops at the same task. I am using a Ubuntu 12.04 VM running on Oracle Virtualbox. Here is my local.conf:

MACHINE ??= 'imx6qsabresd'
DISTRO ?= 'poky'
PACKAGE_CLASSES ?= "package_rpm"
EXTRA_IMAGE_FEATURES = "debug-tweaks"
USER_CLASSES ?= "buildstats image-mklibs image-prelink"
PATCHRESOLVE = "noop"
BB_DISKMON_DIRS = "\
     STOPTASKS,${TMPDIR},1G,100K \
     STOPTASKS,${DL_DIR},1G,100K \
     STOPTASKS,${SSTATE_DIR},1G,100K \
     ABORT,${TMPDIR},100M,1K \
     ABORT,${DL_DIR},100M,1K \
     ABORT,${SSTATE_DIR},100M,1K"
CONF_VERSION = "1"

BB_NUMBER_THREADS = '16'
PARALLEL_MAKE = '-j 16'

DL_DIR ?= "${BSPDIR}/downloads/"
ACCEPT_FSL_EULA = ""
INHERIT += "rm_work"

This is my build configuration:

Build Configuration:
BB_VERSION        = "1.20.0"
BUILD_SYS         = "x86_64-linux"
NATIVELSBSTRING   = "Ubuntu-12.04"
TARGET_SYS        = "arm-poky-linux-gnueabi"
MACHINE           = "imx6qsabresd"
DISTRO            = "poky"
DISTRO_VERSION    = "1.5.3"
TUNE_FEATURES     = "armv7a vfp neon callconvention-hard cortexa9"
TARGET_FPU        = "vfp-neon"
meta
meta-yocto
meta-oe
meta-fsl-arm
meta-fsl-arm-extra
meta-fsl-demos
meta-fsl-arm
meta-fsl-demos
meta-browser
meta-gnome
meta-networking   = "branch:e9f640dce8c13e99ab4d6eecb574d34e26dda958"

I am new to Linux and the Yocto Project, and have been trying to resolve this for days now, so any help would be appreciated. Also if anyone wants to see the whole log file please let me know.

Thanks,
Alvin

Outcomes