AnsweredAssumed Answered

PeX CPU Clock Configurations, the Clock Manager, and the Power Manager

Question asked by LARRY KOOS on Jan 13, 2015
Latest reply on Jan 21, 2015 by Alice_Yang

I'm using KDS 2.0.0 and MQX KSDK 1.1.0.

 

With ProcessorExpert (PeX), one creates clock configurations in the CPU component and picks one of them as the initial configuration. I'm now trying to use the Power Manager to transition from RUN to VLPR states, but it is not clear which PeX 1component you use to create the clock configurations used by the Power Manager and Clock Manager. In fact, I cannot find in the PeX environment where to create multiple clock configurations that are reference-able from the clock/power manager source code.

 

Can someone explain the correct process for creating these configurations and how to make them reference-able?

Outcomes