Is there any way to upgrade an existing node locked perpetual license to get the latest version of the CodeWarrior software?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there any way to upgrade an existing node locked perpetual license to get the latest version of the CodeWarrior software?

Jump to solution
527 Views
WilliamW
Contributor III

I currently have a license for CodeWarrior for ColdFire architectures that will only allow installation of up to CodeWarrior 10.5.  Is there any way to upgrade the existing node locked perpetual license to include the latest (10.6) version?

Labels (1)
0 Kudos
1 Solution
429 Views
TICS_Fiona
NXP Employee
NXP Employee

The license for CodeWarrior v10.5 also works with CodeWarrior v10.6, so you need not upgrade the license in order to use CodeWarrior v10.6.

Fiona Kuang

Technical Information & Commercial Support
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
430 Views
TICS_Fiona
NXP Employee
NXP Employee

The license for CodeWarrior v10.5 also works with CodeWarrior v10.6, so you need not upgrade the license in order to use CodeWarrior v10.6.

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos