Missing DRAM lines

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Missing DRAM lines

Jump to solution
991 Views
olegpereverzev
Contributor I

Hello. In my application I am trying to couple i.MX6 with standard 240-pin DDR3 UDIMM. I've noticed that DDR3 UDIMM specifications imply that you have DQM8 and SDQS8 (and inverted /SDQS8), but there are no such pins on i.MX6. As i understand this can lead to misclocking some chips on DIMM memory device.

Is there any way to fix such trouble? Like duplicating other signal or faking it? Or any other way?

Labels (5)
Tags (3)
0 Kudos
1 Solution
852 Views
Yuri
NXP Employee
NXP Employee

  The 9-th [DQM8 and SDQS8 (and inverted /SDQS8)] is used for checking.
The i.MX6 memory controller does not support it.

~Yuri.

View solution in original post

0 Kudos
5 Replies
853 Views
Yuri
NXP Employee
NXP Employee

  The 9-th [DQM8 and SDQS8 (and inverted /SDQS8)] is used for checking.
The i.MX6 memory controller does not support it.

~Yuri.

0 Kudos
852 Views
olegpereverzev
Contributor I

Thanks. So if I will use non-ECC memory I can ignore those pins?

0 Kudos
852 Views
igorpadykov
NXP Employee
NXP Employee

Probably yes.

0 Kudos
852 Views
olegpereverzev
Contributor I

Thanks, I'll give it a try.

0 Kudos
852 Views
igorpadykov
NXP Employee
NXP Employee

He Oleg

seems it can not be used with i.MX6, in general you can

look at datasheet and try to understand purpose of DQM8 and SDQS8.

I doubt if it can be "duplicated" or "fixed" by some way.

Best regards

igor