Hi,
The command line tools are available under the folder \DSP56800x_EABI_Tools\command_line_tools.
To use it you can for instance launch a command prompt and type directly the tool.exe file.
Example for compiler DSCE
D:\Freescale\dsc 8.0\DSP56800x_EABI_Tools\command_line_tools>mwcc56800e.exe
Metrowerks C/C++ for DSP M56800E.
Copyright (c)1998-2006, Freescale Semiconductor
All rights reserved.
Version 8.1.1 build 1030
Runtime Built: Apr 25 2007 15:26:34
Usage: mwcc56800e.exe [-options]... [files]... [@response]...
Please enter 'mwcc56800e.exe -help' for information about options.
D:\Freescale\dsc 8.0\DSP56800x_EABI_Tools\command_line_tools>
Else you can use a batch file too.
For option an other details please have a look in:
- the txt files in the \DSP56800x_EABI_Tools\command_line_tools folder,
- the 56800x_Build_Tools_Reference.pdf manual,
- the Targeting_56800E.pdf manual.
Hope this will help you.
Pascal