AnsweredAssumed Answered

KBI SP register

Question asked by David Sherman on Jan 7, 2015
Latest reply on Jan 8, 2015 by Mark Butcher

I have an interrupt responding on a KBI interrupt pin.  However, when I look at the KBI_SP register to indicate which pin caused the interrupt, all bits are always set.  This is true even afer I write to the KBI_SC RSTKBSP bit to clear it.  This a MKE06Z128VLH4. I have confirmed that the address is correct for  both the KBI0_SP and KBI1_SP registers, but they are all set and don't appear to change.  Am I missing something?

Outcomes