i am using code worrier 10.2. i develop one barebord application for pxn2020.i can able to run my application in debug mode and its working fine.but when i stop debugging and reset controller program is not there in flash.
i select debug as flash in configuration
why this is happen????
here i attach project....
Original Attachment has been moved to: UARTzip.zip
Hi,
I need to re-install the MCU V10.2.
I don't have the pxn2020 board but a TWR-PXS2010.
I will continue to provide you feedback via the SR 1-3583394090
Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------