The QorIQ SDK (v1.7) uses Yocto to configure and build the required images. However the bitbake recipe (bb) files seem not to fetch the sources from the SOURCE ISO (QorIQ-SDK-V1.7-2041218-yocto/poky/sources but from GIT, FTP or HTTP repositories. This seems so because the SRC_URI definitions in the bb use git://, ftp:// or ftp:// prefixes, e.g.:
poky/meta/recipes-extended/lsof/lsof_4.87.bb: SRC_URI = "ftp://lsof.itap.purdue.edu/pub/tools/unix/lsof/lsof_${PV}.tar.bz2"
meta-fsl-ppc/recipes-kernel/linux/linux-qoriq_3.12.bb: SRC_URI = "git://git.freescale.com/ppc/sdk/linux.git;nobranch=1 "
Our project requires that we can build everything from a local version controlled repository. So I like to know if it is possible to force the SDK Yocto environment to use the sources included at the SOURCE ISO.
Solved! Go to Solution.
Hi,
Thanks for pointing this out.
From SDK 1.7, source iso uses new layout:
meta-cloud-services
meta-fsl-arm
meta-fsl-networking
meta-fsl-ppc
meta-fsl-toolchain
meta-java
meta-linaro
meta-oe
meta-virtualization
poky
sources
sstate-cache
that is, poky layer is separated.
So the right cmd to create build project is: 'source ./poky/fsl-setup-poky -m <board>'.
If run 'cd poky; source . /fsl-setup-poky -m <board>', then the pre-fetched sources cannot be found. You need to modify the DL_DIR in conf/local.conf manually).
BR
Hi,
Tarballs are all stored in the directory defined by DL_DIR
and the build system looks there first to find source tarballs. Yocto Project Reference Manual
The variable DL_DIR is defined in <yocto_install_path>/build_target_release.conf/local.conf
# Source download dir
DL_DIR = "/home/freescale/SDK/QorIQ-SDK-V1.6-20140619-yocto/build_p2020rdb_release/../sources"
See FAQ in Yocto Project Reference Manual:
14.22. | How does the OpenEmbedded build system obtain source code and will it work behind my firewall or proxy server? |
The way the build system obtains source code is highly configurable. You can setup the build system to get source code in most environments if HTTP transport is available. When the build system searches for source code, it first tries the local download directory. If that location fails, Poky tries |
BR
Hi,
Yocto finds the source tarball in local <sdk-install-dir>/sources/ folder firstly, if the source tarball is not in the sources folder, Yocto will fetch the source via internet.
The two packages mentioned by you are available in the sources folder, so normally Yocto should find them in local folder instead of downloading from Internet. Can you please provide more details on how to reproduce the issue?
E.g. Linux distro, the detailed reproduce steps
BR
Liang Lunming,
The first time I tried the Yocto project it was getting sources of the internet. When reinstalling the SDK no sources were downloaded from the internet.
Looking back I found that the first time the build_<machine>_release directory was in the directory <install_path>/poky rather then in <install_path>. The first time I followed the online SDK info and used the command "source ./fsl-setup-poky -m t1042rdb-64b" but because fsl-setup-poky does not exists in <install_path> I changed the current working directory to <install_path>/poky. The second time I followed the instructions displayed at the screen after the installation and used the command "source ./poky/fsl-setup-poky -m t1042rdb-64b" without changing the current working directory..
So the root cause of my problem was a mistake in the online SDK info (/poky is missing).
Regards,
Kees Trommel
Hi,
Thanks for pointing this out.
From SDK 1.7, source iso uses new layout:
meta-cloud-services
meta-fsl-arm
meta-fsl-networking
meta-fsl-ppc
meta-fsl-toolchain
meta-java
meta-linaro
meta-oe
meta-virtualization
poky
sources
sstate-cache
that is, poky layer is separated.
So the right cmd to create build project is: 'source ./poky/fsl-setup-poky -m <board>'.
If run 'cd poky; source . /fsl-setup-poky -m <board>', then the pre-fetched sources cannot be found. You need to modify the DL_DIR in conf/local.conf manually).
BR