P1021 NAND Flash Interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P1021 NAND Flash Interface

542 Views
rajniks
Contributor I

Hi,

I am trying to understand the maximum size of NAND Flash that can be interfaced with P1021. As per the reference manual there are two kinds of page size supported

  • Small page NAND Flash (528 Bytes - 512 bytes as main region and 16 bytes as spare region)
  • Large page NAND Flash (2112 bytes - 2048 bytes as main region and 64 bytes as spare region)

I intend to connect 1GB NAND Flash but it has  page size of 4320 bytes (4096 as main region + 224 bytes as spare region). Please let me know if it is possible to interface chips which have larger page size then the one Ref Manual mentions.

Regards

Raj

Labels (1)
Tags (3)
0 Kudos
1 Reply

366 Views
lunminliang
NXP Employee
NXP Employee

Hi,

I am afraid not mentioning larger size in the reference manual is not support, it's not possible to interface 4K page size NAND to FCM.

regards

0 Kudos