Dear community ,
I hope to download the flash date to the i.MX28 EVK board with MFG tool via usb interface.
Then, Which setting should I select on SW3 ?
S3 switch : USB 5V Power switch
Left position: USB 5V “OFF” / disconnected
Right position: USB 5V “ON” / connected
Best Regards,
Koichi Sakagami
Hi koichi
S3 selection should be coordinated with S16,
it is shown on IMX28_EVK_QUICKSTART p.11
if S16 selects "VDD5V pin is supplied by the USB micro AB jack"
then S3 should be "USB 5V power from the USB micro AB jack is connected
to the EVK board."
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------