UART initialization With RTS CTS signals in K50 subfamily

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UART initialization With RTS CTS signals in K50 subfamily

588 Views
sujaigowda
Contributor II

I just started Kinetis controller. We are using MK50DX256CLL10 in our project and i want to interface UART using RTS,CTS. I want to test UART peripheral without using any driver functions. i want to create Bareboard project.Is there any UART example that shows how to initialize and access UART?

0 Kudos
1 Reply

309 Views
Rick_Li
NXP Employee
NXP Employee

Hi,

I would suggest using Processor Expert to generate an sample project for UART.

Processor Expert is a software tool that integrated into CodeWarrior or KDS and it is very easy to generate the drivers for each module of Kinetis.

CodeWarrior and KDS (Kinetis design studio) both can be downloaded from Freescale web site.

I hope it helps!

0 Kudos