AnsweredAssumed Answered

SPI Chip Select

Question asked by Joseph Chen on Dec 18, 2014
Latest reply on Jan 5, 2015 by jeremyzhou

I'm using Kinetis MCUs. I wonder if it is possible to connect two SPI slave devices shared the same SS line. One of the SS lines contains a NOT logic gate so I can select the slave device by changing its GPIO value in callback function. Is it possible?

Outcomes