Clock source of i.MX6 HDMI TMDS and audio clock.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Clock source of i.MX6 HDMI TMDS and audio clock.

Jump to solution
1,071 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a simple question about the clock source of i.MX6 HDMI TMDS and audio clock.

I guess the clock source of TMDS is video_27m_clk_root from PLL3 PFD1 and HDMI audio clock is regenerated from TMDS with N and CTS.

Is this correct?

Best Regards,

Satoshi Shimoda

Tags (1)
0 Kudos
1 Solution
732 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

I think yes, this is correct.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
3 Replies
733 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

I think yes, this is correct.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
732 Views
satoshishimoda
Senior Contributor I

Hi Igor,

Thank you for your reply.

Then, would you let me know the tolerance of HDMI audio clock which is made by TMDS clock also?

(e.g. +- xx%)

Best Regards,

Satoshi Shimoda

0 Kudos
732 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

please check

IMX6DQ6SDLHDG  Table 2-20. 24 MHz crystal tolerance guidelines

Best regards

igor