Can not enable SRTC on TWR-LS1021A board?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can not enable SRTC on TWR-LS1021A board?

862 Views
nixyeah
Contributor I

The Security monitor has a HP RTC and a SM_LP SRTC.

I noticed that they both can not be enabled on TWR-LS1021A board.

I use uboot SDK 1.3 to test, below are logs:

=> md 1e90000

01e90000: 00000000 00000000 00000000 00000000    ................

01e90010: 00000000 88000b00 00000000 00000000    ................

01e90020: 00000000 00000000 00000000 00000000    ................

01e90030: 00000000 00000000 00000000 00000000    ................

01e90040: 00000000 00000000 00000000 00000000    ................

01e90050: 00000000 00000000 00000000 00000000    ................

01e90060: 00000000 00000000 00000000 00000000    ................

01e90070: 00000000 00000000 00000000 00000000    ................

01e90080: 00000000 00000000 00000000 00000000    ................

01e90090: 00000000 00000000 00000000 00000000    ................

01e900a0: 00000000 00000000 00000000 00000000    ................

01e900b0: 00000000 00000000 00000000 00000000    ................

01e900c0: 00000000 00000000 00000000 00000000    ................

01e900d0: 00000000 00000000 00000000 00000000    ................

01e900e0: 00000000 00000000 00000000 00000000    ................

01e900f0: 00000000 00000000 00000000 00000000    ................

=> mm 1e90038

01e90038: 00000000 ? ffffffff

01e9003c: 00000000 ? .

=> mm 1e90008

01e90008: 00000000 ? ffffffff

01e9000c: 00000000 ? .

=> md 1e90000

01e90000: 00000000 00000000 00007cf8 00000000    .........|......

01e90010: 00000000 88000b00 00000000 00000000    ................

01e90020: 00000000 00000000 00000001 00000000    ................

01e90030: 00000000 00000000 00000000 00000000    ................

01e90040: 00000000 00000000 00000000 00000000    ................

01e90050: 00000000 00000000 00000000 00000000    ................

01e90060: 00000000 00000000 00000000 00000000    ................

01e90070: 00000000 00000000 00000000 00000000    ................

01e90080: 00000000 00000000 00000000 00000000    ................

01e90090: 00000000 00000000 00000000 00000000    ................

01e900a0: 00000000 00000000 00000000 00000000    ................

01e900b0: 00000000 00000000 00000000 00000000    ................

01e900c0: 00000000 00000000 00000000 00000000    ................

01e900d0: 00000000 00000000 00000000 00000000    ................

01e900e0: 00000000 00000000 00000000 00000000    ................

01e900f0: 00000000 00000000 00000000 00000000    ................

It seems that below bits can not be modified, so that the SRTC can not be enabled.

RTC_EN - HP Real Time Counter Enable 0 RTC is disabled 1 RTC is enabled

SRTC_ENV - Secure Real Time Counter Enable and Valid

     When set, the SRTC becomes operational. This bit cannot be changed once SRTC_SL or SRTC_HL bit is set.

     0 SRTC is disabled or invalid.

     1 SRTC is enabled and valid.

Is this because both below are not used?

TA_BB_RTC and RTC_CLK

Tags (3)
0 Kudos
1 Reply

579 Views
nixyeah
Contributor I

Any update on this?

0 Kudos