AnsweredAssumed Answered

TSS 3.1 C++ wrapper question :)

Question asked by kazola on Dec 17, 2014
Latest reply on Jan 6, 2015 by Martin Kojtal

Hi,

I just built the FRDMKL05Z_DEMO_CPP example

However, size is soooo big, close to maximum 32K.

 

   text   data    bss    dec    hex    filename
  26860     48   3644      30552   7758    FRDMKL05Z_DEMO_CPP.elf
  26860     48   3644      30552   7758    (TOTALS)

 

  1. Code optimization is maximum (-Os). Is there a way to shrink the size of this library down? For example, I'm just using ASlider, I do not need Rotary functions, perhaps I can omit them?
  2. Also, does this library contains any code for proximity functions? I think not! Let me know again
  3. Finally, which is the smallest code needed for proximity + touch functions? With Processor Expert and no C++ wrapper I have been able to achieve, around 20 K, as far as I remember.

 

Please let me know your thoughts about the 3 questions! Have a nice day.

Outcomes