Hi,
I am trying to porting the TI WL18XX WIFI Driver in Android-JB on a IMX6 Sololite custom board based on IMX6SLEVK and I have facing some problems.
I am using the Android Jelly Bean of the IMX6SLEVK for my custom board with some changes I had made.
Already the Atheros WIFI if ported in Android Jelly Bean for IMX6SLEVK.
So i applied patches for the Android jelly bean for my custom board. But when i am compiling the Android JB , Only atheros Wifi code is compiled. TI WL18XX WIFI code did not compiled .
I also attached the TI WL18XX WIFI driver patch in this post. Please find it.
Please kindly suggest any ideas to overcome this issue.
Thanks and Regards,
Hi vinothraj
please look at below thread where seems this was solved
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igorpadykov,
Thanks for your quick reply. But I am asking about My added ti wifi driver is not compiled,atheros wifi driver only compiled.
I need to change the makefile which is higher up in the hierarchy which decides what are the drivers to be included. I need to find that makefile. But i do not know where the file is located.
Or how can I find it.
And I just attached the compilation of the ../myandroid/hardware/imx/wlan only
Please find it.
Thanks
vinothraj.
Hi vinothraj
I think better to post that to TI, since they are owner
of TI WL18XX driver.
~igor
Hi igor,
i need to change the makefile where the atheros wifi driver is included in the Android BSP (JB), that is Android BSP (JB) is given by freescale. I want to change atheros to ti wl18xx .
So only i post this question here.
Thanks and regards,
Vinothraj