How work exactly the MFS?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How work exactly the MFS?

Jump to solution
1,268 Views
arnogir
Senior Contributor II

Hello

I'm using MQX 4.1 on K70 with an external Nandflash linked to the NFC.

I open this device and mount a device ("a:") and then use to store a big file resource used by PEG (400 000 Bytes)

Also, for my application, I want save some parameter in a file.

Then I open a file, save some data and close the file.

But after a power off/On, data are note saved in the file. I must close the MFS.

But I think If I close to re open, My PEG resource could not run correctly..

Is mandatory to close the MFS to save definitely a file into the Nandflash?

How work the MFS? When data are realy saved in the nandflash?

Thanks

Labels (1)
0 Kudos
1 Solution
727 Views
arnogir
Senior Contributor II

Hello

Flush memory is the good solution!

View solution in original post

0 Kudos
7 Replies
727 Views
arnogir
Senior Contributor II

Hello

No body to inform me?:smileycry:

0 Kudos
727 Views
arnogir
Senior Contributor II

Is IOCtl Flush will resolved my problem?

If yes, should I do it on file handle or on mfs handle?

0 Kudos
727 Views
DavidS
NXP Employee
NXP Employee

Hi Arno,

Are you running the FFS with the MFS to access NAND flash?

NAND flash requires FFS (flash file system with wearleveling).

FFS has a fflush command using filesystem_handle:

/TASK

0 Kudos
727 Views
arnogir
Senior Contributor II

Hi

I'm using the following code to open the  flash.

if (_io_nandflash_wl_install(&_bsp_nandflash_wl_init, FFS_DEVICE) != MQX_OK) { printf("Can't install FFS!\n"); // _task_block();   } else { if (nandflash_handle == NULL) { /* Open nand flash wl in normal mode */ nandflash_handle = fopen(FFS_DEVICE, NANDWL_OPEN_NORMAL); if ( nandflash_handle == NULL ) { printf("Unable to open NAND Flash device.\n"); printf("\nYou must run \"ffs_repair\" command\n"); return -1; } /* Install MFS over nand_wl driver */ error_code = _io_mfs_install(nandflash_handle, filesystem_name, (_file_size)0); if (error_code != MFS_NO_ERROR) { printf("Error initializing MFS: %s\n", MFS_Error_text((uint32_t)error_code)); return -1; } if (filesystem_handle == NULL) { /* Open file system */ filesystem_handle = fopen(filesystem_name, NULL); error_code = ferror (filesystem_handle); if ((error_code != MFS_NO_ERROR) && (error_code != MFS_NOT_A_DOS_DISK)) { printf("Error opening filesystem: %s\n", MFS_Error_text((uint32_t)error_code)); return -1; } printf ("NAND flash installed to %s\n", filesystem_name); if ( error_code == MFS_NOT_A_DOS_DISK ) { printf("NOT A DOS DISK! Format will start.\n"); error_code = ioctl(filesystem_handle,IO_IOCTL_DEFAULT_FORMAT,NULL); if (error_code != MFS_NO_ERROR) { printf("Format finish with error code 0x%X", error_code); } else { printf("Format finish"); } return 0; } } else { printf("\nNAND flash was installed.\n"); } } else { printf("\nNAND flash device was opened.\n"); } return 0; }

After that I open a file by using path "a:/file.x"...

This answer to your question?

0 Kudos
728 Views
arnogir
Senior Contributor II

Hello

Flush memory is the good solution!

0 Kudos
727 Views
skteh
Contributor III

Hi Arnaud,

How you flush you memory?

I tried fflush(filesystem_handle), but it doesn't save.

After power off, the file gone.

Thankx

0 Kudos
727 Views
arnogir
Senior Contributor II

I do fflush only:

returnCode = fflush(My MQX_FILE_PTR)

Test the return code if return MQX_OK or other?

0 Kudos