AnsweredAssumed Answered

SDCard and Ethernet are not working simultaneously in TWRK60D100M

Question asked by Utsavi Kalpesh Bharuchwala on Dec 13, 2014
Latest reply on Dec 16, 2014 by soledad

Hi,

 

I am working with Codewarrior v10.6 and of MQX v4.0.

 

In my project I am working on  ethernet as well as on SDCard.

 

Problem is both are not working simultaneously in Tower kit. Means  whenever I am inserting SDCard into Tower K60D100M slot, ethernet port is not working in tower((LED on Socket is also not glowing)).When I am removing SDCard from Slot Ethernet Port is working (LED on Socket is also glowing).


I dont know why it is happening??


Is there any jumper setting that I need to do in TWRK60D100M for SDCard??Or is there any settings in userconfig.h file that I need to do??


Please note that both task are working fine individually but not working simultaneously.


I also have seen while using Ethernet SDcard cannot be used but cant get the solution and Link is not able to open.


Please help. 

Outcomes