AnsweredAssumed Answered

MCF52233 Flash program utility for Windows 64 bit

Question asked by Gil Fine on Dec 8, 2014
Latest reply on Jan 29, 2015 by Marc Vandenhende

I use the CF flasher (version 3.1.10) to program MCF52233 on Windows 7 ,32 bit which works fine.

The problem is that CF Flasher doesn't work on Windows 7 ,64 bit.

1. Are there any plans porting it for 64 bit ?

2.If the answer is no, I am interested in another simple utility for programming - for production purposes.

I am looking for a free one, since only basic features are needed (without mass production features).

Is there some free utility by Freescale to program/verify/erase the flash memory?

Thanks,

Gil

Outcomes