AnsweredAssumed Answered

i.mx6sl, MMPF0200 PMIC question

Question asked by KENT MEYER on Dec 3, 2014
Latest reply on Dec 4, 2014 by Vadim Aleynikov

We are planning to use the MMPF0200 with a 3.3V input voltage and suspect

that there will be problems with the SW2 output.

 

Can SW2 operate with 100% duty, i.e. can the SW2 PMOS be persistently

on if/when SW2 is on?

 

Can SW2 correctly operate if its output voltage is set equal to its input voltage

(Vsw2=Vsw2in) and Lsw2=0 (a wire in place of the inductor)?

 

-- Kent

Outcomes