Minimum SPI Delay after Transfer on MPC5644A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Minimum SPI Delay after Transfer on MPC5644A

647 Views
EAlepins
Contributor V

Hi,

 

In MPC5644A DSPI module, CTARn[PDT and DT] can be configured to set a delay inserted between chip select negation and next chip select assertion. As opposed to other timing configurations, the datasheet does not impose any minimum on this value. Can I then assume the smallest that it's possible to configure in the registers will be ok for the MCU? (i.e. PDT=00 and DT=00, which yields a delay of 1 * 2 * 1/fsys)

 

Thanks.

Labels (1)
Tags (3)
0 Kudos
1 Reply

401 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

yes, it is OK for the MCU. It depends rather on slave if it is able to accept such short delay between the chip select assertion.

Regards,

Lukas

0 Kudos