Hello,
I have a question regarding uVision project export from Driver Suite 10.4.2
Micro: PKEAZ128 64 pin.
Keil MDK:
Version 5.12.0.0
Pack: http://www.keil.com/pack/Keil.Kinetis_KEAxx_DFP.1.1.0.pack
Driver Suite 10.4.2
Selected device: SKEAZ128MLH4
I can generate the code in Driver Suite.
To export to uVision I am trying the following;
File->Export
But on clicking finish I get this;
What is my mistake?
Thanks,
John
Solved! Go to Solution.
Thanks Marek,
I have tried a couple of versions of these instructions, none match my installation exactly.
However, I have fixed it.
I had 2 versions of Keil's MDK and 2 version of Processor Expert. So I uninstalled all of them and reinstalled only the latest with the packs I needed.
John.
Hi John,
I am sorry but I cannot see screenshots that you have posted (an error on the page). But I know that there were error in the Keil MDK 5 for SKEAZ family (an error was reported when the exported project was opened by uVision). There is available Freescale Processor Expert Add-On for MDK 5.12 installer that fix the problem, see page Freescale Processor Expert Add-On for MDK 5.12
Detailed instructions (how to install, setup and configure the export ) are available on the web page Using Keil μVision 5 with Processor Expert | MCU on Eclipse.
Best Regards,
Marek Neuzil
Thanks Marek,
I have tried a couple of versions of these instructions, none match my installation exactly.
However, I have fixed it.
I had 2 versions of Keil's MDK and 2 version of Processor Expert. So I uninstalled all of them and reinstalled only the latest with the packs I needed.
John.